Industry Online Support
Technical Forum
3/22/2021 6:15 PM | |
Joined: 3/3/2013 Last visit: 12/19/2023 Posts: 1 Rating: (0) |
Hi everyone! I do have a problem with the "ImportDataRecords". Panel, TP1200 6AV2 124-0MC01-0AX0 There are two recipes, in the panel, with a few datsets each. The export is fine and makes no problem! The export and import are done by a script. Now, the problem is the "ImportDataRecords". I have spoken to the German Siemens Hotline but there is no final solution available. So I am trying my luck here :-) The import should be done by the selction of the previous exported files. The operator should type in the name of the file which should then be imported. The file(s) including already, all the necessary information about the where and what to import. This is the information, as far as I could see, in the already, exported csv file(s). Am I right there? The function is used in an Script. In an IPC the script works fine and I have rewritten the parts for the Panel-Windows CE as described in the Panel manuals of Siemens, differences between IPC and Panel, regarding the script terminology. ImportDataRecords "\Storage Card USB\SLS01",0,Overwrite ,hmiOn,"DB_ExportImportRecipes_ExportStatus" In the script, written in one line! The script is more complex, but even the line above won't work. The file SLS01 is in the root directory of the USB-Stick and is present. I will attache the csv file! PLEASE NOTE: The file needs *.csv as extension to open in Excel! The upload does not allow *.csv! Thanks in advance for the help! Regards Klaus AttachmentSLS01.txt (267 Downloads) |
Last edited by: I DONT WANT A NICKNAME at: 03/22/2021 18:17:31Last edited by: I DONT WANT A NICKNAME at: 03/22/2021 18:20:16 |
|
Follow us on