8/29/2019 11:11 AM | |
Joined: 12/2/2012 Last visit: 5/24/2024 Posts: 7 Rating: (0) |
Hi, In one of the machine Smart Line Module 6SL3130-6AE15-0AA0 is used to power up three Single motor Module.Once there was fault on Smart line module and We used Successor Module 6SL3130-6AE15-0AB1 to replace the old module, Sinamics CU320 RDY Light turned to constant red. So is successor is really compatible with its predecessor? |
8/29/2019 11:20 AM | |
Joined: 12/2/2012 Last visit: 5/24/2024 Posts: 7 Rating: (0) |
SLM is connected via CLIQ interface. So it is communicating with CU320. |
Follow us on