3/19/2007 3:31 PM | |
Joined: 2/5/2007 Last visit: 9/9/2023 Posts: 101 Rating: (10) |
Hi! I have a FB wich I have called eleven times. Since it's using the same instance DB I have been thinking if it's possible to use indirect addressing and only call the FB one time. The reason thatI use the same instance DB is that I can stick to oneWinCC flexible project. I think you will understand what I want to accomplish when you look at the attached pdf. Regards -- Daniel AttachmentIndirect addressing STEP 7.pdf (342 Downloads) |
Follow us on