6/10/2024 5:17 AM | |
Joined: 8/31/2010 Last visit: 8/8/2024 Posts: 1519 Rating: (226) |
Yes, WinCC Unified Engineering software needs to be installed in addition to your current WinCC Unified. You can download the WinCC Unified Engineering software from here. License related details can be found in the system manual. **License wise yes there are different licenses are available. ***However, using WinCC Advanced license, you can still use it to configure Unified Basic Panels, Unified Comfort Panels, Unified PC up to 10K Tags. * System Manual - SIMATIC STEP 7 Basic/Professional V19 and SIMATIC WinCC V19 ** Page no. 8 *** Page no. 369 You can refer Guide for switching from Comfort Panels to Unified Comfort Panels and from WinCC Runtime Advanced to WinCC Unified PC Runtime to know the differences between both the worlds. Yes, this TIA Portal Add-in - Data2Unified helps to convert the Comfort / Advanced configuration contents to Unified. You can familiarize with Unified system using SIMATIC WinCC Unified Tutorial Center (Videos) There are demo projects available, Getting Started manuals, free modernization training (Comfort / Advanced to Unified) available for WinCC Unified system - if you are interested, you can refer this post. |
Like it? Rate it! |
|
7/1/2024 2:57 PM | |
Joined: 5/30/2022 Last visit: 8/8/2024 Posts: 561 Rating: (94) |
Hi, You can download the TRIAL from the following link: SIMATIC STEP 7 incl. Safety, S7-PLCSIM and WinCC V17 TRIAL Download With a WinCC Advanced license you can use WinCC Unified as you can see in the following link in the manual: |
If this information really helps, you could use the Rate function. |
|
Follow us on