5/4/2017 7:51 PM | |
Posts: 4 Rating: (1) |
Thank you for your reply; The license manager is starting up without errors, and no messages. It is also running... |
6/3/2017 10:07 AM | |
Posts: 4 Rating: (1) |
I tried several times to restart, but it does not helps... :-( |
7/6/2017 11:45 PM | |
Posts: 1 Rating: (24) |
Hi, I had the exactly the same issue. Make sure that you run the automation license manager and the TIA portal always as Administrator. If you right-click on the shortcut and go to the file location where the application is installed. You can then right.click on it, select properties and go to the compatibility section. There it is possible to check a "Run as administrator" box. Regards Martin |
This contribution was helpful to40 thankful Users
|
Follow us on