3/7/2018 4:16 PM | |
Posts: 25 Rating:
|
Greeatings, I have one problem and i cant resolve it, I measuring lenght od wood, i need first cut and other cut are which i choose for example 600 mm My problem is , when wood go first cut make interrupt but other dont, Interupt was in same block ob41 an I have measuring in same block logic are diferent Here was my Programm Edit: Please see the attached ZIP-file for the pictures. Can someone help me whay interrupt dont activate when finish first cut ? Attachmentt0r3r0s program.zip (66 Downloads) |
Last edited by: The Helping Hand at: 3/8/2018 2:32:37 PMDeleted links to pictures and put them into a ZIP-file. |
|
3/7/2018 4:57 PM | |
Joined: 12/18/2014 Last visit: 9/1/2024 Posts: 33656 Rating:
|
Oh no..... please archive all pcitures in a ZIP-file and attach the ZIP-file to the post. Edit: in attachment the pictures from the first post. Attachmentpictures.zip (56 Downloads) |
Last edited by: ixo65 at: 3/7/2018 5:02:09 PM |
|
This contribution was helpful to
1 thankful Users |
Follow us on