1/11/2018 8:28 AM | |
Posts: 1 Rating: (0) |
Hello Dave, is it possible to let the IOT2000 work as a PLC using Snap7 to communicate with other actual PLCs? I have an IOT 2020 with an IKHS Power Shield which contains a Galileo Gen 2 Board. I read a lot about reading Data into an IOT from other PLCs but is it also possible to send them back and write data into a PLC? If that's the case, would you rather recomment to use "Settimino" or "Snap7-IOT-Quark" ? Thanks for your help! Best regards. ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 1/11/2018 1:29:54 PMNew subject after splitting Last edited by: fabian.reuschel at: 1/12/2018 7:46:33 AM |
|
Follow us on