12/20/2018 12:51 AM | |
Posts: 3 Rating: (0) |
If we have all the netload over only one port in PLC 1518F-4, in ths case is over interface 1, where you have able 2 ports but we are only using 1 port, so we want to reduse the netload, and a possible solution is to distribute the data traffic in a second port, but for this in TIA Portal you should change the subnet of the port, is possible to maintain the same subnet in bowth ports X1 and X2. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/20/2018 1:56:30 PMNew subject after splitting |
|
12/21/2018 6:33 AM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2986)
|
Hello, yes both ports are the same networkcard. refer the technical data and description of S7-1500 PLC https://support.industry.siemens.com/cs/ww/en/view/86140384 Regards |
Follow us on