6/8/2024 9:02 PM | |
Joined: 12/30/2019 Last visit: 7/3/2024 Posts: 26 Rating: (2) |
I have a question related to this. Would it be possible to send the run/stop command to the webserver from a third party application through an HTTP Post Command. This removes the need for me to login to the Siemens Webserver to run or stop the PLC. I examined the traffic sent on wireshark when the stop/run button is clicked on the webserver and it looks like it's a bunch of HTTP Post commands to run/stop the PLC What I need help with would be how to craft the HTTP Request required Has anyone done something like this? ------------------------------------------------------------------------------------------ |
Last edited by: Oladimgba at: 06/08/2024 21:04:03Last edited by: Jen_Moderator at: 06/10/2024 08:52:59New subject after splitting |
|
Follow us on