4/9/2010 5:53 AM | |
Joined: 1/17/2006 Last visit: 7/4/2024 Posts: 553 Rating:
|
Hello ! Is possible to simulatethis applicationusing PLCSim and Runtime WinCC Flex and save the data logging file generatedon PC ? Greetings. Splitted from Data loggging with trigger bits in Winccflex 05. |
Last edited by: O_Moderator at: 4/12/2010 8:18 AMnew subject after splitting "Educate the children and it won't be necessary to punish the men." |
|
4/12/2010 6:55 PM | |
Joined: 5/13/2008 Last visit: 12/18/2019 Posts: 836 Rating:
|
Hi Pulsar, yes it is possible. Follow the instructions of this FAQ: http://support.automation.siemens.com/WW/view/en/38717202 But use "PLCSIM" instead of "TCP/IP(Auto)"as described in the FAQ. Hint: The interface parameter assignment has to match the WCF settings, for instance use "PLCSIM(PROFIBUS)" if your WCF connection is set to "PROFIBUS". |
mfG / Best regards |
|
This contribution was helpful to
1 thankful Users |
4/13/2010 3:11 AM | |
Joined: 1/17/2006 Last visit: 7/4/2024 Posts: 553 Rating:
|
Hello ! Ok, I understood how to set the interface using PLCSim. I have createdone data log (Data_log_1) with 100 data records perlog, circular method and#10 logs.As a trigger tag I createdTag_1 (M4.0) and Tag_2 is the logging process variable (MD500 as real). So, I want to start (M4.0 =1) and stop (M4.0 = 0)the logging process variable (MD500)with the trigger bitcontrolled byPLC (M4.0).When Iwrite this trigger tag M4.0 to 1 value itmust start the logging process of MD500and stop when the value is 0. I also want to save the data in a PC file. How can I do it ? Please, could someone show me some steps to implement that... Greetings. |
"Educate the children and it won't be necessary to punish the men." |
|
4/13/2010 9:32 AM | |
Joined: 4/24/2006 Last visit: 7/12/2024 Posts: 8711 Rating:
|
Dear Berg, Perhaps this link might give you a hint: how can you store tags/data records event-triggered with date and time in a CSV file? Or you should use the 'events' of the tag M4.0 to start logging and stop logging Best regards, Wizard |
4/14/2010 6:01 AM | |
Joined: 1/17/2006 Last visit: 7/4/2024 Posts: 553 Rating:
|
Hello Wizard !
Thank you for the link, it´s interesting using scripts.
I´m trying to use the events of M4.0 tag to start/stop data logging, but I am not having success at it. Well, I´m using a WinCC Flex Runtime PC to test the application. I have created a Data_log_1 to storage at path C:\test\(TXT file) and two tags: > Tag_1 (Bool M4.0) - Trigger Tag: Properties: Logging> Data Log>Data_log_1 Events: High limit> StartLogging> Data_log_1 Low limit> StopLogging> Data_log_1 > Tag_2 (Real MD500) - Process Tag: Properties: Logging> Data Log> Data_log_1 With these configurations it´s not working. The column "values" in Data_log.TXT file is always 0. I really don´t know what are my mistakes... If someone can help meI´ll appreciate ! Greetings. |
Last edited by: Berg at: 4/14/2010 6:02 AM"Educate the children and it won't be necessary to punish the men." |
|
Follow us on