11/25/2009 10:30 AM | |
Joined: 8/25/2007 Last visit: 6/4/2022 Posts: 13 Rating: (0) |
Hi This info is very useful but itis for PCS7 acting as a slaveto talk to a Modbus master. Is there any examples for configuring the PCS7 to be the Modbus master with standard Modbus CFCs? Thanks |
Last edited by: O_Moderator at: 11/26/2009 9:02 AMnew subject after splitting from /tf/WW/en/Posts/36875#top |
|
11/26/2009 9:50 PM | |
Posts: 2661 Rating: (279)
|
Hi Jeremy, Have a look at the attachments in the following thread: |
11/30/2009 11:38 PM | |
Posts: 2661 Rating: (279)
|
Look at daga's post in the following thread: MODBUS MASTER Regards |
Last edited by: Phantom75 at: 12/1/2009 9:46 PM |
|
12/1/2009 9:44 PM | |
Posts: 2661 Rating: (279)
|
Hi Jeremy, You can download the latest PtP software from the following link: Download CD "CP340, CP341, CP440, CP441" Installing the software will also install example project zXX21_01_PtP_Com_CP34x. Also see chapter 9 in the following manual: CP 341 Point-to-Point Communication, Installation and Parameter Assignment Regards |
Follow us on