3/27/2015 1:07 PM | |
Joined: 1/9/2013 Last visit: 4/7/2024 Posts: 45 Rating:
|
Dear Lucas, With the RDG160KN it’s possible to configure a set point that will change the mode between heating and cooling, Changeover function, parameter 37. For this you have to connect the right sensor to X1 or X2. Fan control: Depending your application you can decide also if the fan should running in heat or cool mode or both. As attachment the basic documentation of this thermostat, have a look on pages 28 and 52 and further. Best regards Richard AttachmentBasisdoc_RDG100KN_en.zip (584 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on