2/9/2020 8:26 AM | |
Joined: 3/16/2015 Last visit: 10/10/2021 Posts: 1250 Rating: (173) |
How about this. |
2/11/2020 2:58 PM | |
Joined: 3/2/2007 Last visit: 5/8/2024 Posts: 929 Rating: (5) |
If we supply the 3RV2922-1CP0 from after the breaker, then it will detect the off by hand? |
... thank you ... |
|
2/12/2020 7:27 AM | |
Joined: 3/2/2007 Last visit: 5/8/2024 Posts: 929 Rating: (5) |
Is the 3VA9988-0AA21 suitable to be mounted on these breakers? 3VA1032-4ED32-0AA0 , circuit breaker 3VA1 IEC frame 100 breaking capacity class S Icu=36kA @ 415V 3-pole, line protection TM210, FTFM, In=32A overload protection Ir=32A fixed short-circuit protection Ii=10 x In nut keeper kit 3VA1040-4ED32-0AA0 , circuit breaker 3VA1 IEC frame 100 breaking capacity class S Icu=36kA @ 415V 3-pole, line protection TM210, FTFM, In=40A overload protection Ir=40A fixed short-circuit protection Ii=10 x In nut keeper kit 3VA9988-0AA21 , LEADING CHANGEOVER SWITCH CHANGEOVER CONTACTS TYPE HP (14MM) ACCESSORY FOR 3VA1 and 3VA20 up to 3VA25 (can this one be mounted on the above two breakers?) |
... thank you ... |
|
2/13/2020 3:58 PM | |
Joined: 3/2/2007 Last visit: 5/8/2024 Posts: 929 Rating: (5) |
So, this is a good combination? 3VA1132-4ED32-0AA0 , circuit breaker 3VA1 IEC frame 160 breaking capacity class S Icu=36kA @ 415V 3-pole, line protection TM210, FTFM, In=32A overload protection Ir=32A fixed short-circuit protection Ii=10 x In nut keeper kit 3VA1140-4ED32-0AA0 , circuit breaker 3VA1 IEC frame 160 breaking capacity class S Icu=36kA @ 415V 3-pole, line protection TM210, FTFM, In=40A overload protection Ir=40A fixed short-circuit protection Ii=10 x In nut keeper kit 3VA9988-0AA23 , LEADING CHANGEOVER SWITCH CHANGEOVER CONTACTS TYPE HQ (7MM) ELECTRONIC ACCESSORY FOR 3VA1 and 3VA20 up to 3VA25 |
... thank you ... |
|
Follow us on