7/15/2019 7:40 PM | |
Joined: 12/18/2014 Last visit: 4/28/2024 Posts: 32897 Rating: (4067)
|
If the RUN / STOP LED is lits red, the expansion module can not communicate with the module on the left. As a rule, the contact slides have dirty contacts. Sometimes just enough simple, multiple back and forth to correct the contact problems. Or spray a electric contact spray on the contacts and then slide the slides back and forth several times. If that does not help, then maybe swap out the expansion modules to determine which module is causing the problems. AttachmentLOGO! 8 manual 0BA8 2017_11 xxxx8-0BA0 page 57.pdf (144 Downloads) |
Last edited by: ixo65 at: 07/15/2019 19:43:37attachment |
|
7/15/2019 7:54 PM | |
Joined: 12/18/2014 Last visit: 4/28/2024 Posts: 32897 Rating: (4067)
|
In the manual nothing is written by flashing red, but only red lit. Maybe you should start a Support Request. |
Follow us on