6/4/2012 11:54 AM | |
Posts: 205 Rating:
|
hI, how to get USS communication library fors71200 plc ???iam usingTIA portal v11... |
6/5/2012 8:34 AM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
Hello, you must install the GSD file for the drive. Regards Christoph |
6/5/2012 8:34 AM | |
Joined: 8/31/2010 Last visit: 7/18/2025 Posts: 1525 Rating:
|
Hello sparten, refer this, which is one of the option Connecting a SINAMICS drive to an S7-1200 CPU in TIA Portal (via GSD file) the other option is using StartDrive v11 software. |
Like it? Rate it! |
|
6/11/2012 6:33 PM | |
Joined: 8/31/2005 Last visit: 9/12/2025 Posts: 2198 Rating:
|
A GSD file is used to add a Slave to a PROFIBUS and GSD(ML) file to add it to a PROFINET Controller. I'm quite shurefor USS you do not need them. I think you just call the USS blocks. The drive on the other side is not configurated in the TIA Portal. Study this exampe http://support.automation.siemens.com/WW/view/en/40157517 (Follow the last link in the link list to a FAQ how to update from V10.5 to V11) |
|
|
6/12/2012 7:34 AM | |
Posts: 205 Rating:
|
HI Ganesh10, thanks for your replay.............. |
Follow us on