5/5/2025 7:25 PM | |
Joined: 5/4/2025 Last visit: 5/6/2025 Posts: 3 Rating:
|
Hello everyone! I'm newbee in the LOGO and have one small project: 1. Push button one time: The Light in the bathroom turn on. If the light is on > 5 min, then the fan is starting to work for 10 min. If the light is on < 5 min, then the fan is not working. 2. If fan is starting to work for 10 min and the light will turn off or turn off and then turn on timer will not be reset. 3. Push button 2 times can stop the fan immediately or start if it didn't work prefer > independently. 4. Long push for 2 sec stop light and fan I have some UDF but can't understand how to add 1 and 2 logics to udf. Q1 - light / Q2 - fan Maybe you have some ideas. Best regards Attachmentswitch1-2.zip (179 Downloads) |
5/6/2025 11:45 AM | |
Joined: 12/18/2014 Last visit: 9/15/2025 Posts: 35964 Rating:
|
Try this.
Attachmentswitch1-2_V2.zip (197 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on