1/19/2017 8:05 AM | |
Joined: 12/18/2014 Last visit: 7/22/2024 Posts: 33391 Rating: (4143)
|
Without load and with load the same voltage? |
1/19/2017 8:19 AM | |
Posts: 8 Rating: (0) |
No my mistake :). It goes from 0 up to 1,2V. ( above 12% the voltage is still 1,2V) // Pierre |
1/19/2017 10:35 AM | |
Posts: 8 Rating: (0) |
There was nothing wrong with Logo, it was the inverter that had wrong settings. The inverter was set for 0-20mA instead of 0-10V. //Pierre |
Follow us on