4/3/2022 4:38 PM | |
Joined: 3/19/2022 Last visit: 5/16/2022 Posts: 10 Rating: (0) |
I forgotted, the LOGO is : 6ED 1052 1M000-0BA8 |
4/3/2022 4:40 PM | |
Joined: 12/18/2014 Last visit: 10/6/2024 Posts: 33883 Rating: (4215)
|
You mean this? 6ED 1052 1MD00-0BA8 |
4/3/2022 6:10 PM | |
Joined: 3/19/2022 Last visit: 5/16/2022 Posts: 10 Rating: (0) |
Yes, exactly ! |
4/3/2022 7:02 PM | |
Joined: 6/11/2019 Last visit: 10/6/2024 Posts: 2281 Rating: (99) |
Hello Ispm, The logo is the smallest problem. You only have to schedule time monitoring when you first trigger the input. This is to prevent glitches from switching the lighting on and off. Thus, the pilot must press the microphone button within a defined time. It is more difficult to connect the logo to the radio. On the one hand, the radio system should not be changed, otherwise the operating license will expire. On the other hand, the signal must be recognized precisely. I can think of the circuit of a light organ from the 70s (see example picture). Instead of the lamp you can connect a relay, which then switches the input of the logo.But this one is just the logo forum.For such a circuit and its adjustment you have to ask someone who is well versed in this topic. But what is not clear to me is how is the light supposed to be switched off again? So I first defined an input in the logo program. greeting Ella_68 AttachmentRadiolight.zip (667 Downloads) |
4/4/2022 6:40 PM | |
Joined: 3/19/2022 Last visit: 5/16/2022 Posts: 10 Rating: (0) |
Thanks, I let you know. |
Follow us on