Industry Online Support
Technical Forum
7/13/2009 10:17 PM | |
Joined: 3/25/2008 Last visit: 1/28/2022 Posts: 232 Rating:
|
Hi mohit. The manuals you are loocking for are in this link. Best regards. |
Keep working! |
|
7/14/2009 5:23 PM | |
Posts: 173 Rating:
|
Check the link to the previous question /tf/WW/en/Posts/32561 You will need the manual pages 55 to 100 at least to understand how to program the LOGO! via the front cursor buttons and ESC & OK buttons. It is much easier to do it via a connection to a PG or PC with the LOGO! Soft Comfort software - there you can see everything that is going on. Also with the software, it is possible to SIMULATE the program to see where mistakes are, without being connected to the hardware OR If connected to the LOGO!, you can do an ONLINE TEST or MONITORING to see if the program functions correctly in the real world. It all depends on the model number of the LOGO!. If you look under the OK button on the front of the LOGO!, the last 4 letters/digits tell you the model number. It will be -0BA0, -0BA1, -0BA2, -0BA3, -0BA4, -0BA5 or the latest version is -0BA6 The software recomended in the other answer will work with any earlier version The earlier versions do not have all the features of the newer versions. So even the online test or simulation might not be possible if the LOGO! that you are trying to diagnose is too old. LASTLY There will be no error messages or anything displayed on the LOGO! screen if they have not been programmed. There are no default error messages. When you can upload the program from the LOGO! to a PG or PC, then you could post it to this forum (under the attachements below after zipping it) then we can help you with it! Cheers Barbarian! |
7/14/2009 5:37 PM | |
Posts: 89 Rating:
|
Thanks Barbarian |
Follow us on