4/20/2022 2:37 PM | |
Joined: 2/11/2022 Last visit: 11/13/2023 Posts: 5 Rating:
|
Good afternoon, At the moment I'm working on connecting a LOGO project (11 logos) with Priva via MODBUS TCP. This is to be able to switch lighting in a building. Previously, the circuit ran via the TIA portal, but our client has expressed the wish to do this via the building management system (Priva). We cannot establish this connection. Does anyone have experience with linking with Priva? Greetings Rik Guten Tag, Im Moment arbeite ich daran, ein LOGO-Projekt (11 Logos) mit Priva über MODBUS TCP zu verbinden. Damit soll die Beleuchtung in einem Gebäude geschaltet werden können. Bisher lief die Schaltung über das TIA-Portal, aber unser Kunde hat den Wunsch geäußert, dies über das Gebäudeleitsystem (Priva) zu tun. Wir können diese Verbindung nicht herstellen. Hat jemand Erfahrung mit der Verknüpfung mit Priva? Grüße Rik AttachmentKopie van HMITags.xlsx (356 Downloads) |
4/20/2022 2:39 PM | |
Joined: 2/11/2022 Last visit: 11/13/2023 Posts: 5 Rating:
|
|
4/20/2022 2:40 PM | |
Joined: 2/11/2022 Last visit: 11/13/2023 Posts: 5 Rating:
|
|
4/20/2022 2:41 PM | |
Joined: 12/18/2014 Last visit: 7/25/2024 Posts: 33414 Rating:
|
Which LOGO!s have you ecaxtly? Please write the article number ... |
4/20/2022 2:46 PM | |
Joined: 2/11/2022 Last visit: 11/13/2023 Posts: 5 Rating:
|
LOGO8 FS4 |
4/20/2022 2:50 PM | |
Joined: 12/18/2014 Last visit: 7/25/2024 Posts: 33414 Rating:
|
Are the LOGO!s and the Priva in the same IP subnet? |
4/20/2022 3:08 PM | |
Joined: 2/11/2022 Last visit: 11/13/2023 Posts: 5 Rating:
|
Yes |
4/20/2022 3:15 PM | |
Joined: 12/18/2014 Last visit: 7/25/2024 Posts: 33414 Rating:
|
I'm sorry, I don't anything from Priva. I can't help you no more. |
Follow us on