7/27/2023 1:58 AM | |
Joined: 10/4/2018 Last visit: 8/29/2024 Posts: 15 Rating: (0) |
Good day to all of you I am working in a logo project an industrial washing machine control using a VFD for the agitation routine. I am having a hard time trying to transfer the program from PC to the Logo I have the following configuration Logo IP Address 192.168.1.17 subnet mask 255.255.255.0 Gateway 192.168.1.254 computer has an IP 192.168.1.20 static or dinamic connected directly to a switch The most frustrating part is that sometimes and i dont know how to explain it just works there is a lan connnection because i can stop and run the logo! and i can set time, i appreciate a lot your comments Attachmentlaundry_v0.zip (321 Downloads) |
7/27/2023 2:16 AM | |
Joined: 12/18/2014 Last visit: 10/14/2024 Posts: 33955 Rating: (4221)
|
Please don't post multiple for the same problem. You post also your problem in this topic (post #12): Can not transfer program with message text from PC---LOGOYour program ist not problem, I can it upload to my LOGO! without any problem. See my post in the other topic. Why do you enter a gateway address? Are the LOGO! and the PC in different subnets? Have you select in the transmission window the correct network adapter? Is the IP address of the LOGO! double awarded? |
7/27/2023 2:46 AM | |
Joined: 12/18/2014 Last visit: 10/14/2024 Posts: 33955 Rating: (4221)
|
The LOGO! must have a fixed IP address. Have you set the IP address of the LOGO! manual? |
7/27/2023 2:50 AM | |
Joined: 10/4/2018 Last visit: 8/29/2024 Posts: 15 Rating: (0) |
Yes, logo has a fixed addres which is 192.168.1.17 subnet mask 255.255.255.0 and nothing for gateway |
Follow us on