10/4/2022 7:36 AM | |
Joined: 3/17/2016 Last visit: 9/26/2024 Posts: 6 Rating: (1) |
hi, how can i put a field in LWE to read/write day of the week from week timer ? |
10/4/2022 9:06 AM | |
Joined: 5/30/2022 Last visit: 9/24/2024 Posts: 582 Rating: (96) |
Hi AutoGn_9550976, I recommend you review the following documentation: You can also check the Set the weekly time application from the following link: LOGO!-Library – Functions for analog value processing and communication I hope this helps you, if not let me know.
|
If this information really helps, you could use the Rate function. |
|
10/4/2022 10:08 AM | |
Joined: 12/18/2014 Last visit: 9/28/2024 Posts: 33845 Rating: (4206)
|
Hallo Hazard_7, it's good to try to help. But it seems you have no knowledge of LOGO! and you post then only some links. This is not helpful. |
10/4/2022 10:25 AM | |
Joined: 12/18/2014 Last visit: 9/28/2024 Posts: 33845 Rating: (4206)
|
You must make seven switch buttons, for every day a one switch buttons. Take a look at attachment. There is an example with LWE V1.1.1 and LOGO! 8.2. In the LSC diagram take a look at the Parameter-VM_Mappiung. AttachmentWeekly timer LWE V1_1_1.zip (530 Downloads) |
This contribution was helpful to1 thankful Users |
11/11/2022 9:34 AM | |
Joined: 3/17/2016 Last visit: 9/26/2024 Posts: 6 Rating: (1) |
Thanks, i solved.....with CHROME it works, with EDGE i have some problem. |
Follow us on