4/16/2013 6:42 PM | |
Joined: 1/28/2009 Last visit: 7/11/2024 Posts: 6844 Rating: (1363)
|
Hello, I also suggest reading the following discussion on tracking an address in an S7 Program: indirect adress tracineBest regards Hamid Hosseini |
4/17/2013 10:26 AM | |
Posts: 41 Rating: (0) |
Hi Marcian I have copied the section of the STL where this input I 0.2 and M 0.2 are found. I did follow Hamids link about the GOTO with memory overlap but it did not reveal anything. The I 0.2 is a real input which is driven from the Hohner shaft encoder. These inputs are used to exactly position a chain driven hoist and adjustments to position are made via the HMI. hope this helps best wishes Steven
Attachmentcounting.zip (34 Downloads) |
4/17/2013 3:28 PM | |
Posts: 41 Rating: (0) |
Gotcha, thanks Marcian |
Follow us on