7/14/2011 1:03 PM | |
Joined: 9/23/2005 Last visit: 4/17/2024 Posts: 4325 Rating: (1424)
|
Hi, see also the FAQ "How do you configure an S7 connection for the OPC server of a PC station in STEP 7 (TIA Portal) V11 to access the data of an S7-1200 over Industrial Ethernet?"athttp://support.automation.siemens.com/WW/view/en/39960679 AttachmentOPC confituration and test steps.zip (266 Downloads) |
Last edited by: Pegaia at: 11/15/2012 11:19 PMDenilson Pegaia |
|
This contribution was helpful to4 thankful Users |
4/25/2013 6:32 PM | |
Posts: 1 Rating: (0) |
Hi, I have followed the steps and the connection with a single S7-1200 has been succesful. Then I create another connection into the same network but I could not monitor the new variables in the OPC. What can I do to fix this trouble?.. Thanks for your help Some images are attached.
AttachmentS7-1200_ connection OPC trouble.pdf (219 Downloads) |
11/26/2015 5:27 PM | |
Posts: 5 Rating: (0) |
When I "Add new device" Im not getting the PC system. Do I need professional? I am running basic. V13 SP1 U2 |
Follow us on