2/14/2020 9:16 AM | |
Joined: 6/30/2014 Last visit: 7/15/2024 Posts: 458 Rating: (87)
|
Good morning Shami, This is an interesting scenario. In your screenshot, it was a good idea to provide us with it, I can see that there is no entry at all for any SQL-DBs; is that right? Now: - My first suggestion would be to download the latest "DokuPack" and to compare the recommended steps in that documentation with the ones you have done. There may be a difference... ... as I am sure that COMOS works just fine and stable. You may test this, on another machine, following the steps from the documentation of COMOS itself. That is fast and easy. - Which is the old version of COMOS on your machine (which works fine) and which is the new one? - Do you have an updated license file for the new version of COMOS, are you getting an error message, maybe with code -2009? If you like and if it is possible, maybe you can open the license file (XML file, no other formats) and post a screenshot of it, maybe hiding the information you do not like to show for privacy. - How did you configure the ODBC connections to the DBs, to the SQL-DBs? Maybe you have a couple of screenshots of that configuration (without cutting those pics), maybe you like to put them in a word file. - Can you use the "@setup" user, which could be the COMOS-Admin, or is this also missing in the list? - Do you have any further information about this issue, which may be interesting/helping? I wish you good luck, SuperPippo |
Follow us on