5/16/2019 1:11 AM | |
Joined: 12/23/2016 Last visit: 4/16/2024 Posts: 6 Rating: (0) |
Hi mr.vithani, We are using master drive for level measurement purpose in blast furnace. Control method is p100-4. We have fixed set point for up and down command i.e. 200 rpm for down and 400 rpm for up. After giving down command it will go at some level where materilm will present and torque is around 45% ,as material go down it will go down with material measurement with torque 16% which I have set in u011.it is normal operation. But right now we are facing problem that Bob( it's level measurement equipment of 100kg made of hard metal.) Is goes up to some fix level of around 1.7 metre and not going down with material. Pls give me ur valuable suggestions.
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/16/2019 12:58:06New subject after splitting |
|
Follow us on