12/16/2022 10:58 PM | |
Joined: 3/27/2021 Last visit: 2/21/2023 Posts: 18 Rating: (0) |
Thank you , but i didn’t quite understand the second proposition, could you please explain more ? |
12/19/2022 8:08 PM | |
Joined: 7/19/2022 Last visit: 10/14/2024 Posts: 400 Rating: (63) |
Hi Badreddine0077, What @0_Einstein is referring to is to configure 7 S7-1200 as I-Device (Configuration and Application of the PROFINET I-Device Function) and in this way only need RT Advanced the other 8 which would be configured as IO-Controller. I attach a picture of the schematic that would result. |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on