4/3/2024 11:26 AM | |
Joined: 4/3/2024 Last visit: 4/3/2024 Posts: 1 Rating:
|
I'm trying to read out data of a janitza prodata 2 device with a siemens s7 1517. I am using the MB client block and the connection to the modbus server is already established. Attachmentpictures_modbus.pdf (138 Downloads) |
Last edited by: Jen_Moderator at: 04/04/2024 07:36:28Text formatting optimized. |
|
4/3/2024 2:11 PM | |
Joined: 9/26/2019 Last visit: 7/5/2024 Posts: 29 Rating:
|
Hi, I see that you are using "Input register", usually is better to use "Holding register". That's not so important cause in Tia portal the mode must be 0. One question: did u tried to start with offset on modbus addresses (-1 or +1)? For ex, if u want to read 40006, try 40005 or 40007 on PLC. Usually, program PC's don't use offset (like ModScan) but you have to put it in Siemens. Also, u can find the same question in this post: https://support.industry.siemens.com/forum/it/en/posts/protocol-error-8384-modbus-tcp/203828 Maybe can help. Let me know, bye! |
Cantonetti Federico |
|
4/3/2024 5:29 PM | |
Joined: 3/28/2010 Last visit: 7/18/2024 Posts: 1050 Rating:
|
What is the link to the janitza prodata 2 device Modbus slave data map with the addresses? |
Follow us on