10/15/2020 3:25 PM | |
Joined: 10/11/2006 Last visit: 4/26/2024 Posts: 5825 Rating: (789) |
Hello, 4.3.3 Synchronization in advance with "MC_GearInPos" using leading value distance (S7-1500T) https://support.industry.siemens.com/cs/de/en/view/109766464 The dynamics of the following axis during synchronization is obtained from the calculated motion profile and the current dynamics of the leading axis. Changes in the dynamics of the leading axis during synchronization are superimposed on the calculated motion profile. This can have the result that the configured dynamic limits at the following axis are violated. This is displayed in the ".StatusSynchronizedMotion.StatusWord" tag. |
With best regards, |
|
This contribution was helpful to1 thankful Users |
Follow us on