Industry Online Support
Technical Forum
7/26/2006 1:24 PM | |
Joined: 4/24/2006 Last visit: 7/12/2024 Posts: 8711 Rating: (1166) |
Hi Roby, Perhaps the following link will help you: http://support.automation.siemens.com/WW/view/en/21063345 Best regards Wizard |
2/21/2007 12:57 PM | |
Posts: 1 Rating: (0) |
Hey guys,
I have been trying to set up s7-200 and Mc45 together. Followed the instructions on the siemens site http://support.automation.siemens.c...345&caller=view Tested my modem with AT commands and it works perfect. The problem is it dont work with the PLC. I used the test program on the siemens site. But i am not able to send or receive any sms. Thats why i a dropping this here. Maybe some of you experienced the same problem and help me through it. thanks a lot |
2/26/2007 8:28 AM | |
Posts: 2930 Rating: (432) |
Hi all, to send a SMS via a GSM modem is no problem. Goto: www.siemens.de/Microset and have a look to the description of Set 5 To receive a SMS and to have Teleservice function with the same GSM-Modem is not so easy. Why? 1. To send/receive SMS messages and have Teleservice function at the same time requires to control the onboard port of the S7-200. For SMS send/receive the port must be switched to "Freeport". But in freeport mode you can not do Teleservice because this requires PPI-Mode. The best way is to use the freeport mode by default. Before you connect with Micro/WIN you have to receive a SMS at the S7-200 and switch the Port to PPI-Mode. Than you can use MicroWIN for Teleservice. 2. Receive a SMS with S7-200 is not easy because of the SMS receive sequence in a GSM modem. There are two different ways to receive a SMS with a GSM modem: A: Receive a SMS and store it on the SIM-Card B. Forward the received SMS directly to the RS232 Port of the GSM modem without storring it on the SIM-Card. A: This requests from the userprogram to connect to the SIM-card, check if a SMS is received, and transmit the last received SMS to the port. Also a handling of the received SMS it self is requested because the number of SMS you can store on the SIM-card is limited and so you have to delete it also. B: You can set the GSM modem to forward the SMS directly to the RS232 interface. This requested to have the onboard interface in Freeport mode. Otherwise you may loose SMS-messages. In any case this is a lot programm code only to handle send/receive SMS-Massages and support also Teleservice. I hope this helps. Regards Helmut |
Follow us on