4/23/2010 4:54 AM | |
Joined: 5/12/2006 Last visit: 8/14/2024 Posts: 22343 Rating:
|
Hello, here is the FAQ for global Measuring Inputs: http://support.automation.siemens.com/WW/view/en/29063656 You must use Telegram 391/392 to use the global Measuring Input. Regards Christoph |
This contribution was helpful to
1 thankful Users |
4/24/2010 2:40 AM | |
Joined: 1/17/2006 Last visit: 7/4/2024 Posts: 553 Rating:
|
Hello Christoph, Thanks for your answer and link, but I tried the steps suggested in the FAQ, more specifically in the topic 2.4.9 - Error Elimination, but when I try to do the step #5 (Load the configuration to the D4xx and the SINAMICS Integrated with "load project to target system". Activate the option "copy RAM to ROM after loading") the same error appearsin theoutput box ( Error --- There is no configuration of a free telegram for the I/O: 'measuring_input_1: LogAddress' (address: PI278.2) and the download is not completed.
Hello Greg, Could you explain with much details this method you´ve mentioned ?? I couldn´t find P448 in CU Expert list ! Regards. |
Last edited by: Berg at: 4/24/2010 2:41 AM"Educate the children and it won't be necessary to punish the men." |
|
4/26/2010 1:54 PM | |
Posts: 31 Rating:
|
Berg, P448 is a parameter in the Drive's Expert list, not the CU. JakitGT |
4/27/2010 5:56 AM | |
Joined: 1/17/2006 Last visit: 7/4/2024 Posts: 553 Rating:
|
Hello Christoph, First, thank you for your patience and help ! So, I did what you have suggested and the file is attached here. I also have attached some PrntScrn files together to further understanding of the situation. Best regards. AttachmentSimotion_D435.zip (309 Downloads) |
"Educate the children and it won't be necessary to punish the men." |
|
Follow us on