Industry Online Support
Technical Forum
12/2/2013 10:51 AM | |
Joined: 4/14/2010 Last visit: 8/6/2024 Posts: 525 Rating: (11) |
Dear Siwarexi, please see attached, Many thanks, problem was wrong connection, now i have connected according the load cell model WL260 SP-S AB as mention in attached. But i didn't recieve the measurment value in kg i have applied the force on load cell platform the following parameter in SIWATOOL are checked...??? Average Value filter = checked Limit frequency = fg=2Hz Characteristic Value = 2mV/V adjustment weight = 0 zero digit = 0 weight unit = kg Thanks, AttachmentDesktop.zip (151 Downloads) |
Last edited by: O_Moderator at: 12/2/2013 1:02 PMnew subject after splitting from /tf/WW/en/Posts/96577#top MS |
|
12/2/2013 1:04 PM | |
Joined: 4/24/2009 Last visit: 8/2/2024 Posts: 2682 Rating: (135) |
Thread closed, because question is already published in the following thread Without conneting the loadcell Siwarex U giving the SF whats reason..? Best regards O_Moderator |
Follow us on