12/5/2020 9:01 PM | |
Posts: 44 Rating: (0) |
Hello I use micromaster 440 (5.5kw) for a motor(3kw) to lift a load . Usual load is 500kg , The problem is , in lifting up or down , every time when I do RUN command to inverter, the load moves without control , If I send up command to inverter , first the load goes down and then comes up . I need when I sen up command , the load comes up without any movements to down . When I send down command , the load comes down but without speed of inverters ' frequency . it comes down by it's weight (the speed of down movement is high because of load weight ) till I release the down command , at this time the brake stops the load . my mean is , the frequency of inverter and it's torque , has not affect on down movement of load . Whatever I have done is in attached file (My back up of inverter's parameters and a pdf file that I did some changes on the parameters according it ) Please guide me to solve this problem . Regards AttachmentMicromaster backup .zip (412 Downloads) |
Last edited by: hossein82 at: 12/05/2020 21:07:38Last edited by: hossein82 at: 12/05/2020 21:08:12 |
|
Follow us on