12/11/2015 3:52 PM | |
Posts: 1 Rating:
|
Hi, I have a problem with a machine in a local factory in Sweden. The plc has broken down, i need to change the cpu and the panel. its an integrated C7 plc+panel My problem is that the panel is made with protool . I need to migrate the panel project to wincc flexible 2008 SP2, I have not access to SP2 any more just SP3 on my Win7 computer I there any chance that maybe somebody can do the migration for me in this forum?? Please Attached the project The project contains four plcs and four panel. The one I need help with is 1.OP RB-51AH AttachmentJacAtria.zip (486 Downloads) |
12/11/2015 9:17 PM | |
Joined: 3/30/2011 Last visit: 8/7/2024 Posts: 734 Rating:
|
Hello, I make conversion of the 4 panel in the project. Converted file are too big. I put the zip file in dropbox. this is the link. look also the conversion log for some warnings.
Regards |
★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★ |
|
This contribution was helpful to
1 thankful Users |
12/11/2015 9:29 PM | |
Joined: 12/18/2014 Last visit: 8/9/2024 Posts: 33515 Rating:
|
|
This contribution was helpful to
1 thankful Users |
11/24/2016 10:19 AM | |
Posts: 3 Rating:
|
hi Everybody. I have here a Project in Protool. Could someone help me migrate to Wincc flexible 2008 Project. Thank a lot in advanced!
AttachmentKettenofen.zip (370 Downloads) |
11/24/2016 10:21 AM | |
Posts: 3 Rating:
|
Hello Mindware! Could you please help me to migrate a Protool Project into Wincc flexible 2008 SP2 Project. Thanks a lot in advance! AttachmentKettenofen.zip (399 Downloads) |
11/24/2016 10:38 AM | |
Joined: 8/3/2009 Last visit: 8/9/2024 Posts: 13506 Rating:
|
hello caophan in the attachments you will find your project in WinCC flexible 2008SP2 (just HMI without PLC, just reintegrate it) If it helps, don´t forget to Rate! Bye Murof Attachmentkettenofen_flex2008SP2.zip (534 Downloads) |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
11/24/2016 11:27 AM | |
Posts: 3 Rating:
|
Thanks Thanks Thanks a lot!!!!!!!!!!!!!!!!!! |
This contribution was helpful to
1 thankful Users |
Follow us on