9/11/2015 6:05 AM | |
Joined: 5/9/2015 Last visit: 2/5/2024 Posts: 81 Rating:
|
Hello, I have PCS7 V8.1. we have order the 6ES76566CL301BF0 package redundant automation system. In the hardware configuration through wizard i have selected the same MLFB number as mentioned above. The CPU selected by the wizard in the above package are with MLFB numbers 6ES7410-5HX08-0AB0 / V8.1. But the cpu delivered to us are with MLFB number are with 6ES7654-5CL00-0XF0. we are not able to find this MLFB number in the catalog. I have tried the HW update as well. Please suggest how the CPU with MLFB number 6ES7654-5CL00-0XF0 can be available in the CPU list. Best Regards Naresh Saini ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 9/11/2015 2:08:59 PMNew subject after splitting |
|
9/11/2015 7:36 PM | |
Posts: 3 Rating:
|
Hi nkr, 6ES7656-6CL30-1BF0 ist a SIAMTIC PCS 7 CPU 410 Redundancy automation system already asseblemed and tested with 2x CPU 410-5H process automation incl. AS RT PO 100... (See here) 6ES7654-5CL00-0XF0 is a SIMATIC PCS 7 CPU 410-5H Bundle PO 500...(see here) So as you can see it's not the CPU, it's a bundle 6ES7410-5HX08-0AB0 is the MLFB of the CPU 410-5H stand-alone (see here) -> the MLFB number in your catalog is the right one. Regards, Heisenberg__ |
Last edited by: Heisenberg__ at: 9/11/2015 7:37:51 PM |
|
This contribution was helpful to
1 thankful Users |
Follow us on