3/18/2022 8:55 AM | |
Joined: 3/11/2019 Last visit: 1/21/2025 Posts: 1653 Rating: (307) |
Hi, i asume, it is not possible to read/write values directly from/to IW/QW over modbus. The values have to be stored in a data block at least. So you have to read the values from the analog card inside the cpu-1200 and store the values into a datablock. Afterwards the modbus communication must be set with the data accordingly. Maybe this FAQ can help. How do you program and parameterize Modbus/TCP communication between S7-1500 CPUs and S7-1200 CPUs?
regards sancruz |
Feedback appreciated, please rate |
|
Follow us on