4/12/2016 10:39 AM | |
Joined: 10/31/2014 Last visit: 7/1/2024 Posts: 58 Rating: (5) |
Dear All, Can Any one know which block use for Module level diagnose in pcs7 V8.1.??? |
4/12/2016 12:38 PM | |
Joined: 3/14/2008 Last visit: 7/12/2024 Posts: 2076 Rating: (930) |
Hello, Do you mean the channel blocks? - Pcs7AnIn - Pcs7AnOu - Pcs7DiIn - Pcs7DiOu They are the connection between the hardware address and the software blocks. Info from help Signal-processing blocks
Various types of channel blocks are provided in this PCS 7 library for processing signals from inputs and outputs:
This applies to the following blocks: Pcs7AnIn Pcs7AnOu Pcs7DiIn Pcs7DiOu Pcs7DiIT These blocks are used only for processing the signals of S7-300/400 SM modules. Use these standard blocks if you want to optimize memory and runtime utilization and do not need to process any PA devices. FF/PA channel blocks
This applies to the following blocks: FbAnIn FbAnOu FbAnTot FbDiIn FbDiOu These blocks are designed especially for use with PA field devices and the PROFIBUS 3.0 Class A and B or with FF field devices. In particular, you should use these blocks if you want to make use of the special features of these devices. In contrast to standard channel blocks, PA channel blocks not only process the signal itself but also all variables, according to the desired device configuration selected in the hardware configuration.
|
If I could help you, you can use the RATE button. Thank you. |
|
4/13/2016 11:09 AM | |
Joined: 6/14/2006 Last visit: 6/17/2024 Posts: 301 Rating: (60) |
Hi, as we are in the PCS 7 tree of the forum I assume that you talk about PCS 7 OS when you say SCADA. So please refer to: Application example "PCS 7 in Practice - Plant Asset Management": https://support.industry.siemens.com/cs/ww/en/view/56285991 Manual "SIMATIC Process Control System PCS 7 Maintenance Station": https://support.industry.siemens.com/cs/ww/en/view/109485949 for more information about integrated Asset Management of PCS 7. If you have still more questions regarding this topic please come back here... Regards |
4/14/2016 9:00 AM | |
Joined: 10/31/2014 Last visit: 7/1/2024 Posts: 58 Rating: (5) |
hello, without create and update diagnostic screen is it possible to get tag for module or channel level diagnostic? |
Follow us on