9/8/2011 5:59 AM | |
Joined: 1/28/2009 Last visit: 4/26/2024 Posts: 6838 Rating: (1359) |
Dear hazem Check the following tips extracted from the STEP7 online help.
Best regards AttachmentVAT.zip (1186 Downloads) |
This contribution was helpful to1 thankful Users |
9/8/2011 7:35 PM | |
Joined: 1/28/2009 Last visit: 4/26/2024 Posts: 6838 Rating: (1359)
|
Dear hazem To extend the size of process image , you be sure the CPU supports this option.To do so, you should go to H.W config CPU's properties-->cycle,clock memory--> and change size of process-image input area or process-image output area. Also check the attachment.
The reason of peripheral addressing is fully discussed here: Where and when do you need peripheral addressing?
Best regards |
This contribution was helpful to4 thankful Users |
Follow us on