3/2/2010 10:05 AM | |
Joined: 4/24/2006 Last visit: 8/21/2024 Posts: 8719 Rating:
|
Dear isurya, Please have a look at this link: MP277 now with non-volatile Memory and new order numbers
Please tell us, which cable do you use? Best regards, Wizard |
3/2/2010 12:26 PM | |
Joined: 4/24/2006 Last visit: 8/21/2024 Posts: 8719 Rating:
|
Dear INDRA, Let's try to help:
No, the programm will not be lost. The difference of Non volatile memory is because of use WinAC MP277. This option can only be used when (1AX1), because when power loss not only programm is not lost, there are also some actual values of SoftPLC (WinAC MP)are retained.
The difference is frame geometry, see this link: MP277 8" Touch and MP277 10" touch with new frame geometry available now So it depends, which one you want to use.
Perhaps the following link, might help: how can you transfer a WinCC flexible project via MPI/Profibus to a windows based panel? Best regards, Wizard |
3/2/2010 2:12 PM | |
Joined: 4/24/2006 Last visit: 8/21/2024 Posts: 8719 Rating:
|
Dear INDRA, Here is link to manual: SIMATIC HMI HMI device MP277 (WinCC flexible) In the appendix, you will find the different alarm numbers. Best regards, Wizard |
Follow us on