4/23/2015 11:34 AM | |
Posts: 3 Rating: (0) |
Bonjour a tous,
Translation: Hello everyone, I need help with a MP 277 - 10" Touch, for x reasons I lost the software in the HMI and the operating system. At this moment I don't have a white screen with display: Thank you to all of you. David
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 4/23/2015 2:19:17 PMNew subject after splitting and add translation |
|
4/23/2015 3:14 PM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello Automation_David, Have you already tried with this: how do you do an operationg system update (OS update) on operator panels? When power up the MP have you always blank screen? Take a look: MP277 blank screen problem - Entries - Siemens Industry Online ... |
Last edited by: Ste39 at: 4/23/2015 3:17:33 PM |
|
4/23/2015 3:38 PM | |
Joined: 8/3/2009 Last visit: 4/25/2024 Posts: 12869 Rating: (1641) |
Hello Automation_David Then you can only do an OS Update with factory Reset. It is also possible if the panel annot run into the WindowsCE. look in this FAQ: https://support.industry.siemens.com/cs/ww/en/view/19701610 Use the Manual for Prosave. But if you have a Multi Panel you must use a PPI MultiMaster Cable (RS232 or USB). You can find a table in the Manual which Cable do you need. But only with the right Cable you can reset your Panel. I hope i can help. wish you the Best. Bye Murof ----------------- If the Information helps you, you could use the Rate Button |
If this Information really helps, you could use the Rate function |
|
Follow us on