Industry Online Support
Technical Forum
10/10/2008 9:48 AM | |
Joined: 4/24/2006 Last visit: 5/8/2024 Posts: 8638 Rating: (1151) |
Dear picengineer, Have you tried to perform an OS update using option 'Booting' or 'Reset to factory settings' selected? Have a look at this link: http://support.automation.siemens.com/WW/view/en/19701610 See point 5. It's only possible if you use RS232/PPI multimastercable Best regards, Wizard |
10/10/2008 2:39 PM | |
Posts: 4 Rating: (0) |
Wizard Thank you for the reply. I did an OS update via ethernet, I believe you can use ethernet in addition to RS232. Does this reinstall Windows CE or just the siemens application on the device? Also, I am running sm@rtservice and sm@rtaccess on this panel. I used to be able to connect via internet explorer on my PG, but since these symptoms have been occuring, when I log onto the MP370, i get the "no input" icon on my PG. Previously, the last client to log onto the MP 370 would get control and any other client gets the "no input" icon. Very strange. John |
10/10/2008 3:57 PM | |
Posts: 4 Rating: (0) |
Wizard thanks again, I realized that the boot option is unavailable via ethernet OS update. I will try the serial cable method now. John |
Follow us on