9/5/2008 5:48 AM | |
Posts: 487 Rating: (36) |
Hi Cant map internally,but can 'attach' PC drive.No need for license. Have a look at the following two pic's . One is from the (In our case) OP277 control panel (should be similar)Ok besides that you also have to give your network adaoter an IP adress( I can't get it to work on name only IP)and a gateway for different VLAN. The other pic is from inside the winccflex project . We use Smart@ccess ( vnc type thing) with enables us to view/modify screen or even download project. Eric AttachmentOP270connecttoPC.zip (270 Downloads) |
9/5/2008 8:38 AM | |
Posts: 3 Rating: (0) |
So, I try to summarize Instead of sending the data to a local drive of the MP370, i can send it to the share of another PC. (\\device\share), this must be coded in my application 1) What happens if there is a network problem? 2) Do I really need smart@ccess or can I do it without smart@ccess? |
9/5/2008 10:05 AM | |
Posts: 487 Rating: (36) |
1- A network problem .... is a problem because usualy it stops writing ( no I don't have proper solution . The software we use to extract the text from the info file sends me an email when there are no new alarmlog and datalog in a 24 hour period) 2-You can do without no problem Eric |
2/26/2018 2:39 PM | |
Joined: 6/19/2017 Last visit: 6/28/2024 Posts: 8176 Rating: (169) |
New question published by akendre is split to a separate thread with the subject How to configure 'HMI MP370 network setting' so that it can send data to PC which having operating system 'windows7 Enterprises'?. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on