6/10/2024 7:10 AM | |
Joined: 1/21/2013 Last visit: 8/4/2024 Posts: 3044 Rating: (479)
|
Hi eng.t.saleem, It may help to test on a different subnet. I have seen some problems in the past because the two network interfaces have to use different subnets, but during an image upgrade with factory reset, you can only assign the IP address to the interface you are using. If there is a conflict with the other interface, no communication will be possible. If this does not help, I recommend that you contact technical support. Kind regards |
Follow us on