10/25/2010 3:50 PM | |
Posts: 5 Rating:
|
Plz Help...I was doing OS Update on my new spare TP177A with MPI/Profibus settings within the network of s7300 & TP177A(connected with profibus cable) & PG/PC Connected to S7-300 with Direct serial cable with 3-3,4-4,5-5,9-9 connections at back of profibus connector on s7-300 cpu. Suddenlly my PG/PC Laptop went into sleep mode and while trying to restore the process got interrupted in between due to which now my new TP177A is not booting. It is always show blue screen with "bootloader 1.8, 2006/11/10" written at left side of screen and that blue screen remains there for ever. 1. Now i tried to OSupdate with "Reset Factory Options" on ProSave/Wincc both but not able to communicate. 2. i tried serial/ppi cable setting also for this OSupdate with "reset..." but not able to connect. 3. a screen comes and keep on asking to boot the HMI...but nothing happens beyond that. 4. Now situation is that i am having only rs232 cable & the cable said above(with 3-3,4-4,5-5,9-9 connections) i tried with both but no results. i cant buy PPI master cable for the time being. plz help me and suggest me which serial cable connections i can try for communication with TP177a and the settings also. Also can i do this bootstraping/reseting on profibus network??
Splitted from Boostrapping and OS update. |
Last edited by: O_Moderator at: 10/26/2010 1:15 PMnew subject after splitting |
|
10/28/2010 1:16 PM | |
Joined: 4/24/2006 Last visit: 4/24/2025 Posts: 8965 Rating:
|
Hello, I do not know if it is possible with "normal" RS232 - RS485 convertor. I think it is not possible Here is link to manual: SIMATIC HMI HMI Device TP177A, TP177B, OP177B (WinCC flexible) See chapter 12.8 for description of interfaces. Best regards, Wizard |
3/15/2017 2:11 AM | |
Posts: 1 Rating:
|
Hello I have a problem with the same subject. Is it possible to do factory settings with the cp5512 adapter?
|
Follow us on