4/30/2012 6:30 AM | |
Joined: 3/3/2008 Last visit: 10/5/2023 Posts: 333 Rating: (51) |
hi try this one whether its the same you are having? regards ram Attachment611u_39.zip (301 Downloads) |
This contribution was helpful to1 thankful Users |
5/2/2012 10:57 AM | |
Joined: 9/18/2006 Last visit: 8/6/2024 Posts: 590 Rating: (64) |
Hi. AttachmentExample_nContr_S120.zip (283 Downloads) |
This contribution was helpful to1 thankful Users |
5/2/2012 12:22 PM | |
Posts: 8946 Rating: (999) |
Thank you, dear friend. But this project is language locked, would you please save again in universal language? Please have a look here: http://support.automation.siemens.com/WW/view/en/22635866 |
5/2/2012 12:41 PM | |
Joined: 3/21/2006 Last visit: 7/26/2024 Posts: 10228 Rating: (1181) |
Hello pfuser, In oder to open it properly can you explain which of bellow mentioned software packages need to be installed on PC:
1.PDM 2.Protool 3.WinCC FLex 4. Starter Are all of them used? IBN-Serviceopen the project folder (path:\1M660_07\Global and delete file with name Language. Aggreed that the correct way is your mentioned above. Best regards, Hristo Mihalev |
Last edited by: UMENCHO at: 5/2/2012 12:44 PMLast edited by: UMENCHO at: 5/2/2012 12:41 PM |
|
5/2/2012 1:33 PM | |
Joined: 9/18/2006 Last visit: 8/6/2024 Posts: 590 Rating: (64) |
Hi. I also sometimes have to open other people's projects - Removed global / languare.* Best regards. AttachmentExample_nContr.zip (267 Downloads) |
This contribution was helpful to2 thankful Users |
5/2/2012 1:35 PM | |
Joined: 9/18/2006 Last visit: 8/6/2024 Posts: 590 Rating: (64) |
Hi. I use: WinCC FLex, Starter. Best regards. |
Last edited by: pfuser at: 5/2/2012 1:36 PM |
|
This contribution was helpful to1 thankful Users |
Follow us on