10/29/2020 3:40 PM | |
Joined: 5/5/2015 Last visit: 4/7/2024 Posts: 15 Rating: (0) |
Hello Sir, Please advice where can i get the firmware files for below said control unit. 6SN1118-0NJ01-0AA0 Version A A5E00108638 Firmware card part number is A5E00228755 V 07.02.06 When I power up the unit display shows E-A001. Please help & send me the exact link to download the exact firmware file. Please do the needful at the earliest. Machine is in breakdown condition. BR Kiran ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/30/2020 08:48:20New subject after splitting |
|
10/30/2020 11:27 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Please refer this link SIMODRIVE 611U / POSMO SI/CD/CA V7.2 software package.& refer SIMODRIVE 611 universal SIMODRIVE 611 universal E, Control Components for Closed–Loop Speed Control and Positioning manual chapter 4.3.5 for firmware download procedure. HTH |
Last edited by: Jen_Moderator at: 10/30/2020 12:04:31Optimized links. |
|
10/30/2020 2:10 PM | |
Joined: 5/5/2015 Last visit: 4/7/2024 Posts: 15 Rating: (0) |
Hello Sir, Thanks for your quick reply & expert advice. If i click the first link there are many exe files to download. Do i need to download only posmo_070206.exe(446 KB) file? Please advice. Awaiting your quick reply, BR Kiran |
10/31/2020 4:34 AM | |
Joined: 10/17/2007 Last visit: 9/17/2024 Posts: 4031 Rating: (353)
|
You need to download "Toolbox" and unzip it to find out 611U firmware
|
Last edited by: nulizhang at: 10/31/2020 04:36:36If you like my comments please |
|
10/31/2020 5:27 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello Kiran, Please download & read documentation_a0703.exe file. Then check Simucom U software version installed on your PC/PG, if it is latest version, its OK or else please download simocomu_070206.exe & installed this on your PG/PC. You can search l& upgrade the latest Simucom U on web latter on also, for time being to load firmware use the above link. Then download toolbox_070204.exe file on your PG/PC & then try to download it to 611U drive. HTH. |
11/2/2020 4:32 AM | |
Joined: 10/17/2007 Last visit: 9/17/2024 Posts: 4031 Rating: (353)
|
Update my answer --You need to follow the link (which you saw many xx.exe files) --to download "611u_0702xx.exe" --unzip it, found in the package--611u.ufw. By the way, I just did the same thing for my customer today (Nov. 01) who had a 611U control card needing a firmware upgrade to V.6.1. I did this in less than 40 min's some tips: #1--the link you mentioned is for version V7.2, If you need other ver. you can search on Siemens web.here #2--SIMO COM U version may not same but needing higher than 611u.ufw version #3--My SIM COM U version is V14. my customer old ver. is V1.1--I don't know yours my 611U card is an encoder feedback type (NH); yours is resolver feedback (NJ) #4--Upgrade --download by SIM COM U to 611U taking 3 to 5 min's make sure no power interrupting during download #5--you can download firmware to a USB storage then copy to you Laptop to unzip. It is better. I don't suggest unzip in the Win10 or Win 7 PC. If my answer helps, please use the "rating" button
|
If you like my comments please |
|
11/2/2020 8:02 AM | |
Joined: 5/5/2015 Last visit: 4/7/2024 Posts: 15 Rating: (0) |
Hello Sir, Good Morning, Thanks for your expert advice. I am using Simocom U Ver 14.03.02 & my laptop OS is WinXP Sr. Pack 3. I have downloaded the toolbox_070204.exe file & extracted but i cannot find firmware files in it (.ufw, cfw) Please help Awaiting your quick reply. BR Kiran |
Follow us on