11/6/2019 5:43 AM | |
Joined: 8/18/2019 Last visit: 7/5/2024 Posts: 32 Rating: (0) |
Dear sir, can you send me manual of 6ra80 dcm drive for controlling speed and read write parameter via telegram configuration ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/06/2019 11:54:43New subject after splitting Regards, |
|
11/6/2019 8:22 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (875) |
Hello, There is no any ready made example of Sinamics DCM control via any controller. You may refer SINAMICS DCM DC converters, Operating Instructions, Firmware Version V1.5 for DCM operation manual & SINAMICS DCM, List Manual, Firmware version 1.5 (based on 5.1 SP1) manual for configuration of telegram types information.. Please refer SINAMICS DCC: Positioning and synchronism with SINAMICS DCM and CU320-2 application example for more information. HTH |
Last edited by: Jen_Moderator at: 11/06/2019 12:25:25Optimized links. |
|
11/6/2019 10:34 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (875) |
I guess sina_speed & sina_para are for TIA & not available with DCM. Please refer attached sheet (extracts from Siemens Sinamics DCM list manual) having information of types of telegrams & connections which can be configured in DCM profidrive communication set up. HTH AttachmentDCM telegram types & connection details.pdf (199 Downloads) |
11/6/2019 2:44 PM | |
Joined: 4/28/2015 Last visit: 9/20/2022 Posts: 1278 Rating: (296) |
Hi, from the list I can see that telegram 1 is supported, so I expect that SINA_SPEED FB will work for SINAMICS DCM. Or you can also use telegram 352 with the according block from the LSINAExt library: https://support.industry.siemens.com/cs/ww/en/view/109747655 |
Best regards, |
|
11/11/2019 11:00 AM | |
Joined: 8/18/2019 Last visit: 7/5/2024 Posts: 32 Rating: (0) |
Thanks For your valuable replay |
Regards, |
|
Follow us on