3/31/2020 6:10 PM | |
Posts: 46 Rating: (0) |
Hi, my situation is a bit different. Flow sensor gives 15 Hz per 1m/s waterspeed i need the water flow in l/sec or l/min knowing that the tube internal diamer is 42mm Therefor i have the K-factor (K-Factor is the number of pulses a sensor produces for one liter of fluid measured) In my project K-factor is equal to 11,78 pulses/l water So 1 puls=0.084l water I can not folow the calculation in the post above 1/4500 should be 0,00022222 in stead of 0.222 l, or did i miss something ? hope someone can help me out. ------------------------------------------------------------------------------------------ |
Last edited by: Yves-M at: 03/31/2020 18:25:55Last edited by: Yves-M at: 03/31/2020 18:36:38Last edited by: Jen_Moderator at: 04/01/2020 06:45:23New subject after splitting |
|