1/26/2024 8:58 AM | |
Joined: 5/30/2022 Last visit: 10/1/2024 Posts: 582 Rating: (96) |
Hi nnnayeem, Which S7-1500 do you have, for example a 1511 can only connect 10 panels, as you can see in the technical data (number of connections section) the first thing is to check that the PLC has the capacity to connect so many HMI panels: CPU 1511-1PN, 300KB Prog., 1,5MB Data After this I understand that you are going to connect a SWITCH/ROUTER to connect all the panels to the PLC.
|
If this information really helps, you could use the Rate function. |
|
1/31/2024 12:15 PM | |
Joined: 8/3/2009 Last visit: 10/11/2024 Posts: 13911 Rating: (1757)
|
Hello nnnayeem I think you should have a look at this FAQ: https://support.industry.siemens.com/cs/de/en/view/109479986 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on