5/27/2021 4:14 AM | |
Posts: 1 Rating:
|
Good day Sir, Many thanks for your time to review below issues. I have a SIMATIC PCS 7 CPU 410E REDUNDANCY SYSTEM (6ES7656-6EK30-1GF0) with SIMATIC MODBUS/TCP PN RED and additional CP cards for Modbus communication. 6AV6676-6MB30-4AX0 SIMATIC Modbus/TCP Red for S7-400 H systems, Single license on CD ON 6GK7443-1EX30-0XE0 Communications processor CP 443-1 (firmware V3.2) May I know whether I need to use 6AV6676-6MB30-3AX0 on this CP or 4AX0? Currently there is any issue on DCS (EMERSON) communication interface using CP cards 1. The primary network communicates well. However, communication is disconnected in the secondary network every 1 mintues based on DCS reponse time 500ms(default). 2. Even if we change the DCS response time from 500ms to 5000ms, the disconnection of the secondary network is similar. Only the interval of disconnection of the secondary network becomes longer. 3. Even in the Modbus test program by “Modbus Poll”, “Message Time-out” was occurred when the response time was with 2100ms or 2200ms, less than 2500ms. 4. We have tested communication with other systems such as Honeywell several times with S7-400H CPU412H, 414H, and so on, and so far there is no problem. Is there any problem when using PN MODBUS network and CP MODBUS network together in S7-400H CPU410E? Much appreciate if you can advise this case. ------------------------------------------------------------------------------------------ AttachmentNetworks Sketch - Copy.pdf (665 Downloads) |
Last edited by: Jen_Moderator at: 05/27/2021 09:18:31New subject after splitting |
|
5/30/2021 12:44 AM | |
Joined: 9/1/2017 Last visit: 6/9/2024 Posts: 156 Rating:
|
Hi
Please have a look at Which technical data applies for the SIMATIC Modbus/TCP blocks and for which CPUs and CPs is it released .
Hope this helps |
Last edited by: Jen_Moderator at: 05/31/2021 09:20:35Optimized link. |
|
Follow us on